-
Click “Project Project Information”.
The “Project Information” dialog opens.
-
Select the “Automatically generate 'Project Information' POUs” option.
Example
Requirement: The following property is defined.
Schlüssel = nProp1 Typ= Zahl Wert= 333
-
Select the “Automatically generate 'Project Information' POUs” option.
-
Declare a
DINTtype variable.Example:
showprop : DINT; -
Call the function
GetNumberProperty:showprop := GetNumberProperty("nProp1");You are granted access to the value in the application.
Note: The functions that are created with the “Automatically generate 'Project Information' POUs” option can be used only if the runtime supports the WSTRING data type. If this is not the case, then instead you can apply the “Automatically generate 'Library Information' POUs” option. You can use the functions created in this way at least in the application
to access properties. These functions are not registered in the runtime.